I use HMC703 and HMC736
pfd=10M
RFout=14.75G
using frac mode
when i use adisimpll to simulate ,it can't lock
BW 40KHz
phase margin 60
how can i lock to my frequency
HMC703
Last Time Buy
The HMC703 fractional synthesizer is built upon the high performance PLL platform also contained in the HMC704 and Hittite’s latest generation of PLL...
Datasheet
HMC703 on Analog.com
HMC736
Recommended for New Designs
The HMC736 is a GaAs InGaP Heterojunction Bipolar Transistor (HBT) MMIC VCO. The HMC736 integrates a resonator, negative resistance device, varactor diode...
Datasheet
HMC736 on Analog.com
I use HMC703 and HMC736
pfd=10M
RFout=14.75G
using frac mode
when i use adisimpll to simulate ,it can't lock
BW 40KHz
phase margin 60
how can i lock to my frequency
ADISimPLL indicates a lock condition after about 160us but to see a decrease in phase error you must increase the simulation time to 350us. This is similar to your other post at HMC703+HMC632 .
i use hittite-eval-software to control my circuits on my pcb,it can't lock too,but it locked to my wanted frequency.the ld_sdo shows '0' ,however i change other register.
If the part is locked but you do not see a logic "1" on LD_SDO check Reg 0x0F=0x81. This turns on the lock detect output.
i have checked,but it still did not lock
i solved this problem,change CPoffset to 0mA ,then LD_SDO='1'
Good to hear it now locks. With 10MHz comparison frequency, Fout=14.75GHz and Icp=2.54mA the offset current should be 91uA (Reg 0x09=0x24BFFF). The lock detector window size should be 51ns ( Reg 0x07=0x2CD).