Post Go back to editing

HMC966LP4E Image Rejection

Hi all,

Our customer evaluate the HMC966 RF performances.

Frequency is ,

・LO=10GHz , +6.5dBm

・RF=18GHz

・IF=700MHz

Following the measurement setting is Typical Application Circuit at the datasheet 12 page.

SG(RF) - isolator - HMC966 - 90 deg Hyblid(IF) - filter - Spectrum Analyzer

SG(LO) - isolator -

Our customer measurement data of Image rejection is the data sheet specifications as well as the 15dB, but it is minimum spec.

Customer target spec is 20dB(min) w / design margin.

What we are thinking that ,

Is it possible to improve the performance by adjusting the line length between the IF1/IF2 output and the 90 deg Hyblid ?

Do we have other way to improve the performance of the Image rejection ?

Best regards,

sss