KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
HMC1106
Recommended for New Designs
The HMC1106 is a double-balanced mixer, which can be used as an upconverter or a downconverter, with DC to 24 GHz at the IF port, 20 to 50 GHz at the LO...
Datasheet
HMC1106 on Analog.com
Hello all,
I could not find IF Return Loss Response data of HMC1106 in the datasheet.
Could you please provide IF Retrun Loss Response data of HMC1106, such as the sample below ?
Thanks in advance.
Hi,
Here is the IF return loss data.
Thanks,