Post Go back to editing

HMC832 PLL

Thread Summary

The user inquires about a PLL with VCO integrated for a 960MHz to 1220MHz band, +3dBm output power, <30usec frequency hop time, -140dBm/Hz phase noise at 1MHz, 60dBc spurious (preferably 70dBc), 10KHz step size, and a 50MHz reference. The final answer confirms that both HMC830 and HMC832 can meet these requirements, but a tunable reference and manual tuning are necessary to achieve the -60dBc spurious and hop time. Phase noise at 1220MHz is around -144dBc/Hz using the HMC830 default eval board loop filter.
AI Generated Content

I’m looking for a PLL with VCO integrated having the following behaviors:

Band: 960MHz to 1220MHz

Pout: +3dBm

Frequency settling time plus writing time of the registers for changing  frequency (time for changing frequancy): <30usec for a hopping  distance equal at 63MHz

Phase noise@1MHz:-140dBm/Hz

Spurious: 60dBc (better if it is 70dBc) 

Step size: 10KHz

Frequency reference: 50MHz

I'd like to know if the HMC832 or the HMC830 can meet the above requarements.

Best regards

Parents
  • Both HMC830 and HMC832 will meet these requirements but the application must utilize a tunable reference and manual tuning to meet the -60dBc spurious and hop time requirements.  I've attached an appnote on manual tuning.  With a fixed 50MHz reference Figure 21 in the HMC830 datasheet shows at frequencies close to  2GHz VCO frequency (1000MHz output) IBS spurs for some channels near the integer boundary could reach -50dBc.  With tunable reference the spur levels drop below -100dBc.

    Phase noise simulations at 1MHz offset for both parts (1220MHz output) is around -144dBc/Hz using the HMC830 default eval board loop filter.

    Fast_Frequency_Hopping_Application_Note.pdf
Reply
  • Both HMC830 and HMC832 will meet these requirements but the application must utilize a tunable reference and manual tuning to meet the -60dBc spurious and hop time requirements.  I've attached an appnote on manual tuning.  With a fixed 50MHz reference Figure 21 in the HMC830 datasheet shows at frequencies close to  2GHz VCO frequency (1000MHz output) IBS spurs for some channels near the integer boundary could reach -50dBc.  With tunable reference the spur levels drop below -100dBc.

    Phase noise simulations at 1MHz offset for both parts (1220MHz output) is around -144dBc/Hz using the HMC830 default eval board loop filter.

    Fast_Frequency_Hopping_Application_Note.pdf
Children
No Data