Post Go back to editing

ADRF6620 PLL locking frequency and Spur

Hi, I am using ADRF6620-Evalz board to test performance of ADRF6620's internal PLL LO signal's phase noise and spurious emission performance.

Here is what I did.

-Connect 20MHz PLL reference clock signal to REFIN port of evalz board

-Set desired LO frequency on ADRF6620-EVALZ software.(2000MHz)

-Enable LO_DRV_EN bit in Register 0x01, Bit 7. to check LO signal

-Connect LO out port to spectrum analyzer to see internally generated LO signal's phase noise and spur.

Here is the result I get from this test.

Too many spurs were generated.  ( attached CSV file of this  measured data)

So I checked Lock_detect signal at MUXOUT pin on EVALZ board(to see if it shows logic high, indicating PLL is locked). There was no signal on this lock_detect pin, which means it probably failed to calibrate PLL frequency.

Is there a way to lock LO frequency and remove spurs?

Please advise.

Thank you,

Grace

Trace_0028.csv.zip