HMC1087-Die and HMC1087F10 has different coupling at RF out on their datasheet. Could you confirm that RF out is AC coupled at HMC1087F10 and at its evaluationboard?
HMC1087F10
Production
The HMC1087F10 is an 8W Gallium Nitride (GaN)
MMI C Power Amplifier which operates between 2 and
20 GHz, and is provided in a 10-lead flange mount
package...
Datasheet
HMC1087F10 on Analog.com
HMC1087-Die
Production
The HMC1087 is an 8W Gallium Nitride (GaN) MMIC Power Amplifier which operates between 2 and 20 GHz. The amplifier typically provides 11dB of small signal...
Datasheet
HMC1087-Die on Analog.com
HMC1087-Die and HMC1087F10 has different coupling at RF out on their datasheet. Could you confirm that RF out is AC coupled at HMC1087F10 and at its evaluationboard?