ADL5331 P-1dB

Hello.


Do you have P-1dB performance characteristics ?
I want High and Low Frequency performance.
And  I want to compare ADL5330 and ADL5331.

Thank you.

Parents
  • There is no p1dB data in the ADL5331 datasheet. The two parts are similar though. If you compare Figure 20 in the ADL5331 datasheet with figure 38 in the ADL5330 datasheet you can get a sense for their comparative saturation powers. However, these two plots are at different frequencies (100 MHz for ADL5331 and 900 MHz for ADL5330).

Reply
  • There is no p1dB data in the ADL5331 datasheet. The two parts are similar though. If you compare Figure 20 in the ADL5331 datasheet with figure 38 in the ADL5330 datasheet you can get a sense for their comparative saturation powers. However, these two plots are at different frequencies (100 MHz for ADL5331 and 900 MHz for ADL5330).

Children
No Data