Post Go back to editing

ADRF6620 MUXOUT output level

Hello,

I would like to confirm ADRF6620 MUXOUT pin's output level.

The pin is configured by register REF_MUX_SEL(0x21).

Question

1, If the MUXOUT is selected "LOCK_DET" or "VPTAT", is the MUXOUT pin voltage same as 3.3V logic level?

2, If the MUXOUT is selected "REFCLK/x", is the MUXOUT pin same as REFIN input level?

Thanks and best regards,

Jun

Parents Reply Children
No Data