Can you provide a sample of set of baseband data coming from the ADF5904, that is then being digitized by the ADAR7251? I am assuming it's just the target delta frequency over time?
Regards,
Will
Can you provide a sample of set of baseband data coming from the ADF5904, that is then being digitized by the ADAR7251? I am assuming it's just the target delta frequency over time?
Regards,
Will
The default settings in SW is set to run 5ms 200MHz triangular ramp.
With these settings and based on radar beat equation
and a target at 3m
The resultant beat frequency will be 800Hz
The default range on the plot is 600kHz so the 800Hz tone may not be visible.
The range can be adjusted by using the highlighted area.
You can also open the Time Domain Display to view the time domain output line on the oscilloscope plot.
Hi, why would the distance be 3m? Apologies i don't understand where the 3m comes from.
Hi, why would the distance be 3m? Apologies i don't understand where the 3m comes from.