Post Go back to editing

ADA2200 Question

Dear Sir/Madam,
I use ADA2200 for testing in a project , and  need to measure the sensor input signal 's amplitude and phase .
1 . B ecause input singla could not guarantee constant within a short time , I want to use 2 ADA2200 to realize above function , one is for phase detection , another piece is for orthogonal   detection, I do not know whether it is avail able ?
2 . Because it is best to use sine excitation for the sensor excitation , RCLK goes through 3-order active low - pass filter into sinusoidal ( frequencies 4KHz ) , is this solution available ?
Thanks.
Parents
  • Dear brianharrington,

    Thank you very much for your answer!Sorry,I have a few questions to ask.
    1. I understand the square wave reference demodulation of the same frequency square wave
    signal when the odd harmonic to bring the noise increase is 1dB, and convert the ADA2200
    output using an ADC with a synchronous sampling clock, using the ADC's digital filter to
    suppress Harmonic noise. So in order to better reduce the demodulation back to the DC odd
    harmonics, I ADA2200 before adding an 8th-order, lowpass filter (such as MAX297), this can?

    2. 2 ADA2200 in the same phase and quadrature measurement need to share the same clock,
    and ADA2200 reset, device is configured to generate a clock if a crystal or resonator is
    placed between the XOUT and CLKIN pins, then the ADA2200 can directly receive the external
    clock Do not have to set the register 0X0028 bit1 bit is 1? Otherwise, through the SPI
    configuration can not guarantee two ADA2200 difference of 90 °.
    3. If the ADC with a synchronous sampling clock is used to suppress the even harmonic
    spurs of the PSD output, then the quadrature phase-locked output of the two ADA2200s also
    requires two simultaneous clock ADCs(such as 2 AD7192),right?

    4. I used to do with the AD5933 organic micro-conductivity measurement, AD5933 although is
    used to measure the impedance, but it is a sinusoidal output excitation, and its signal
    processing is DFT, and finally through the results of the excitation frequency of the
    complex impedance Data, which have phase information, I think that if the AD5933 output
    sinusoidal signal to modulate the LED light source, then the I / V conversion, and then
    input to the AD5933 by BPF, then AD5933 will DFT, the final output of the corresponding
    complex Impedance data, through the complex impedance data can be calculated phase
    information, This is easier to handle than the ADA220 case, I do not know this method to
    detect the phase is appropriate?

Reply
  • Dear brianharrington,

    Thank you very much for your answer!Sorry,I have a few questions to ask.
    1. I understand the square wave reference demodulation of the same frequency square wave
    signal when the odd harmonic to bring the noise increase is 1dB, and convert the ADA2200
    output using an ADC with a synchronous sampling clock, using the ADC's digital filter to
    suppress Harmonic noise. So in order to better reduce the demodulation back to the DC odd
    harmonics, I ADA2200 before adding an 8th-order, lowpass filter (such as MAX297), this can?

    2. 2 ADA2200 in the same phase and quadrature measurement need to share the same clock,
    and ADA2200 reset, device is configured to generate a clock if a crystal or resonator is
    placed between the XOUT and CLKIN pins, then the ADA2200 can directly receive the external
    clock Do not have to set the register 0X0028 bit1 bit is 1? Otherwise, through the SPI
    configuration can not guarantee two ADA2200 difference of 90 °.
    3. If the ADC with a synchronous sampling clock is used to suppress the even harmonic
    spurs of the PSD output, then the quadrature phase-locked output of the two ADA2200s also
    requires two simultaneous clock ADCs(such as 2 AD7192),right?

    4. I used to do with the AD5933 organic micro-conductivity measurement, AD5933 although is
    used to measure the impedance, but it is a sinusoidal output excitation, and its signal
    processing is DFT, and finally through the results of the excitation frequency of the
    complex impedance Data, which have phase information, I think that if the AD5933 output
    sinusoidal signal to modulate the LED light source, then the I / V conversion, and then
    input to the AD5933 by BPF, then AD5933 will DFT, the final output of the corresponding
    complex Impedance data, through the complex impedance data can be calculated phase
    information, This is easier to handle than the ADA220 case, I do not know this method to
    detect the phase is appropriate?

Children
No Data