Find a typical register configuration for integer division.
Now no matter how many of the registers of the N divider ,the vco are oscillating at around 7.5GHz.
Phase frequency is 10MHz and reference input is 50MHz.
The following is my register configuration:
02h <= 5d(R divider is 5)
03h <= 770d(N divider is 770,expected RF out is 7.7GHz)
04h <= 0
05h <= 50894C
06h <= 703387
07h <= 4FA
08h <= 31DF
09h <= 900000
0Ah <= 0
0Bh <= 72
0Ch <= 0
0Dh <= A