Hi All,
Currently, I am considering to form the system for prototyping UWB system based on FMCDAQ2 board. However, I would like to be able to shift signal in the frequency range up to 6GHz.
Could you also advise me does analog devices has wideband (up to 1GHz bandwidth, ideally 1GHz) IQ modulators and IQ demodulator, with a frequency range up to 6Ghz?
In case there are no devices with such and specifications could you provide me suggestions for alternatives.
Kind Regards,
Tarik
Hi,
I am thinking to make direct conversion Tx/Rx. Ideally, I would place a signal on 3.5GHz and occupy bandwidth from 3GHz to 4GHz.
Ideally, I would place a signal on 3.5GHz and occupy bandwidth from 3GHz to 4GHz. It would be nice if I could be able to change central frequency.
Thx,
Hello,
Please take a look at ADRF6780 IQ UC as a good example for integrated solution:
http://www.analog.com/en/search.html?q=HMC8192
as well as the HMC8191 for IQ passive mixer:
http://www.analog.com/en/products/rf-microwave/mixers/iq-and-image-reject-mixers/hmc8191.html#product-overview
Thank you
Hello Gokhan,
You can send me more info on this email: tarik.kazaz@gmail.com.
I would appreciate that a lot, as we are currently in a phase of signal development.
Probably we would need order HW in Q4 of this year.
Hello Tarik,
We are releasing two new demodulators that has a demodulation bandwidth of 2 GHz in RF. Can you send me an e-mail, so that I can share more info on it?
Regards,
Gokhan