Hello everyone,
I am using two HMC1060LP3E but I have problems or misunderstanding of the Enable signal.
First HMC1060LP3E Enable voltage => 182 mV => HMP is OFF
Second HMC1060LP3E Enable voltage => 465 mV => HMP is ON
The datasheet says : "Enable Input EN Low Level 0 to 0.8 V"
I think the second should be OFF as well but it is always ON. Is there anything I missed ?
Thanks in advance!