Post Go back to editing

In-circuit Test Parametric for hmc1118 and ADRF5040

Hi ,

I would like to have a simple testing at In-circuit Test for hmc1118 and ADRF5040.The objective is only test the swicthing is functioning.

1. can I source DC volatge at "RFC" pin and expect same DC voltage at "RF1" or "RF2" ? What is a limit of the DC voltage.
2. can I source sine wave with 10kHz at "RFC" pin and expect same frequency at "RF1" or "RF2" ? what is a minimum frequncy source , RMS value and also current setting.

or any other suggest on this testing

Thanks and regards

BK