Post Go back to editing

HMC850LC3 - typical value of current on VR pin

What is typical current into V_R pin on the HMC850LC3? Is it a function of V_R voltage? Is there data available on Current into V_R vs DC @V_R voltage level?

  • Hi,

    I moved your question in RF and Microwave community. would be able to help you.


    Regards.

  • Hi,

    Usually 2-3 mA is drawn from VR pin to adjust gain. The relation goes linear such that as the VR is increased more current is drawn. We dont have a characterisation for VR current vs voltage specifically for this part but an easy implementation would be choosing appropriate VR for your application  and inserting a series resistor to create a voltage drop referenced to the supply of the IC(for this case, insert a resistor between GND and VR)

    Sinan 

  • According to the data sheet, positive or negative values of VR can be used. I feel like the resistor method cannot work for both. I am more concerned with generating positive VR values (higher Vptp out)

    Please confirm that I am understanding correctly. Are you saying that a constant 2-3 mA is sourced from the VR pin (pos current coming out of pin) regardless of resistor placed? In other words, If I would like to see +.4 V on the VR pin, could I just place a properly sized Potentiometer to gnd on the VR pin and tune accordingly to get desired VR value?

    Thanks,

    Greg

    S

  • Since the part is biased between GND and -3.3V, resistor method can only be used for VR<=0V values. If you want to apply a poisitive VR(0.4V i.e.) you need an external positive supply and a resistor to create drop to adjust 0.4V. Sourced current is constant with respect to VR voltage and current is always drawn from that pin. 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.