Post Go back to editing

HMC349ALP4CE and HMC8038

I reviewed the specifications for HMC349ALP4CE and HMC8038. I understand that HMC8038 is newer.
We would like to use one of these switches at 10MHz. The signal is not a pure sine tone, but is closer to the square way.
Thus, the subharmonics will extend to higher frequencies, let's say up to 80-100MHz.
The datasheets specify Fmin at 100MHz however all the graphs show high isolation and low insertion loss all the way to DC?
Digikey and Mouser and even Analog web site specify these switches as 0-4GHz and 0-6GHz.

The data sheets disagree.


Can I use these parts at 10MHz?

HMC349ALP4CE Datasheet and Product Info | Analog Devices 
http://www.analog.com/media/en/technical-documentation/data-sheets/HMC8038.pdf

If there is a strong objection to using one of these switches what would you recommend instead?

Thank you.

Parents
  • Hello,

    Thank you for the clear and relevant answer.

    I was wondering about this. The datasheet doesn't show data on P1dB and IP3 at low frequencies and hence our uncertainty. We are not planning to use the switches above 13dBm, so large signal degradation is not important to us. However very high isolation will be useful.

    Regards.

Reply
  • Hello,

    Thank you for the clear and relevant answer.

    I was wondering about this. The datasheet doesn't show data on P1dB and IP3 at low frequencies and hence our uncertainty. We are not planning to use the switches above 13dBm, so large signal degradation is not important to us. However very high isolation will be useful.

    Regards.

Children
No Data