For the HMC7590, what is the voltage range and current consumption for the VOVCTL pin and DCA pin? Also, does the VOVCTL voltage influence the analog bandwidth of the HMC7590?
HMC7590
Obsolete
The HMC7590 is a high-speed, high gain, low-power limiting transimpedance amplifier (TIA) used in optical receivers with data rates up to 43 Gbps. It features...
HMC7590 on Analog.com
For the HMC7590, what is the voltage range and current consumption for the VOVCTL pin and DCA pin? Also, does the VOVCTL voltage influence the analog bandwidth of the HMC7590?
VOVLCNT pin and DCA pin can have voltages between 1.6V and 3.3V. The current dissipation should be less than 1mA and they shouldn't affect the analog bandwidth.
VOVLCNT pin and DCA pin can have voltages between 1.6V and 3.3V. The current dissipation should be less than 1mA and they shouldn't affect the analog bandwidth.