Post Go back to editing

AD8313 evaluation board

Hi

I am using AD8313 evaluation board having (AD8313 and OPAMP AD8009)

http://www.analog.com/media/en/technical-documentation/data-sheets/AD8313.pdf 

My questions are:

1.  The frequency range for AD8313 is 0.1 GHz to 2.5 GHz and AD8009 1 GHZ as per datasheet.

Then how the Evaluation board will run more than 1 GHz frequency?

2. I have given two tone input signal at INHI, VPS2=+5V, VPS1=+4V, GND=VNEG=ground.

I have to operate it into LOG (RSSI) mode so I did not make any changes on the evaluation board, because I believe it is configured  by AD in this mode.

There is confusion regarding switch position, The given link have image of board

https://media.digikey.com/Photos/Analog%20Devices%20Photos/MFG_AD8313-EVALZ.jpg 

Which is position A and B (Near VNEG is it A or B) ?

3. For two tone test signal configuration given in 2  is used, and I have tested the voltage across R5 which is summarized as follows:

I/P power (dBm)      Voltage (V)

-65                                 0.69

-50                                 0.80

-35                                 0.95

-15                                 1.42

-10                                 1.52

-5                                   1.62

Is the above range is right or wrong?

I have to take this output and give to a DAC but the DAC i/p voltage is 512 mv peak to peak.

To interface with DAC I require conditioning circuit so that voltage vary between 0 to 512 mV.

If you have idea of conditioning circuit then please let me know.

Thanks a lot..

Girish

Parents
  • 1. AD8009 is on the output of the device. AD8313 provides an output voltage (dc if the input level is fixed) that is proportional to the size of the input signal. So AD8009 is not seeing a 2.5 GHz signal.

    2. According to the schematic, the switch should be in position A which grounds PWDN and enables the part. You are getting an output signal from the part so assume that the switch is in the right position.

    3. Yes and no. To get the board to work correctly, I think that you need to put a negative supply on VPS2. When AD8009 is operated on a single supply its output voltage is only rated to swing down to 1.1 V. So your low end data is non linear because of AD8009.

    4. You can scale down your output voltage by putting a resistor divider on R5 and R6.  If your output is not changing fast, I think that it's safe the connect the resistor divider directly to the ADC. Keep the resistors on the small side though.

Reply
  • 1. AD8009 is on the output of the device. AD8313 provides an output voltage (dc if the input level is fixed) that is proportional to the size of the input signal. So AD8009 is not seeing a 2.5 GHz signal.

    2. According to the schematic, the switch should be in position A which grounds PWDN and enables the part. You are getting an output signal from the part so assume that the switch is in the right position.

    3. Yes and no. To get the board to work correctly, I think that you need to put a negative supply on VPS2. When AD8009 is operated on a single supply its output voltage is only rated to swing down to 1.1 V. So your low end data is non linear because of AD8009.

    4. You can scale down your output voltage by putting a resistor divider on R5 and R6.  If your output is not changing fast, I think that it's safe the connect the resistor divider directly to the ADC. Keep the resistors on the small side though.

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.