Post Go back to editing

How does the RF Amplifier's current change with temperature?

Hello everyone?
I have a question about the data sheet of HMC441LC3B and HMC451LC3.

In the data sheet, it is not possible to confirm the amount of change of the current due to the temperature change.


When the test conditions are as follows, how much current does the current change from room temperature?
1. The power supplied to the RF Amplifier is fixed at + 5.0V and the chamber temperature is -40 ° C.
2. The power supplied to the RF Amplifier is fixed at + 5.0V and the chamber temperature is + 85 ° C.