ADRF6602 - PLL no 'locked'

Dear Sirs,

since four years we used the ADRF6602 as a down-converter. LO freq. = 1605,425MHz. We never changed the hardware (PCB) and also the software was never changed. The converter worked fine the hole time. Now - arround four years later a problem appears: arround 40% of the used chips can't lock the PLL after init the register. Here are some hints related to this design:

# Ref. is a 40.0MHz Oscillator / The level at the ADRF6602 is arround 100mVss + Bias DC ( I also changed this level up to 1Vss - no changes)

# I used the tool "Analog Devices ADRF6x0x Customer Evaluation Software v6.1.0" to configure all registers. The output of this tool (Hex dump) is used by a little controller to program the ADRF via SPI. Here is the output :

REG0: 00 01 40

REG1: 00 32 01

REG2: 00 06 CA

REG3: 70 00 0B

REG4: 0A A7 A4

REG5: 00 00 6D

REG6: 1E DD 8E

REG7: 00 00 07          

# the programming order is (as discriped in your datasheet):

0) after power up: delay 1second before start init

1) write to REG5: PLL disabled

2) delay (150ms to 500ms used - no changes )

3) REG5: PLL enabled  (delay 100us)

4) REG7 (delay 100us)

5) REG6 (delay 100us)

6) REG4 (delay 100us)

7) REG3 (delay 100us)

8) REG2 (delay 100us / up to 200ms tested)

9) REG1 (delay 100us / up to 200ms tested)

10) delay (150ms to 500ms used - no changes )

11 ) REG0        (init finished)

12) delay (150ms to 500ms used - no changes )  .. for VCO recalibration

13) check "lock detect"

---------

# A downconverter which works showed:

- a "Vtune" voltage of 2.002V (f out = 1605,41914 MHz)

-  A power consumption @5V (total, include 2 pre-amplifer and a micorocontroller) 244mA before / 268mA after init

- Vtune at scope looks like figure22 in your datasheet (LO freq. vs. lock time)
MUX out (lock detect) = stable 'high'

# A downconverter which doesn't works showed:

- a "Vtune" voltage of 3.046V (f out = 1634,754 MHz) (not stable)  (Example!)

-  A power consumption @5V (total, include 2 pre-amplifer and micorocontroller) 230mA before / 255mA after init

- MUX out (lock detect) : a 'low' and mostly a short "high" every 100us. This is the same time as seen as Vtune ramp-up time. Which means that the Vtune voltage rises from 0V to >3V in arround 100us.

# I shorted the Vtune voltage to see what the max. VCO range is. All boards produce a broad frequence range much MHz below and above the needed LO-frequency.

# I switched the "VCO Band Select ans SW Source" from "Band cal" to SPI and offer different values to the "Band select".

I found that the value decimal "49" was closed to the needed frequency - but also in this case the chip doesn't 'lock'.

# Here are some samples (LO frequency) - produced by the same hardware and software (programmed: 1605,425MHz):

1885,0 | 2265,0 | 1185,0 | 2267,5 | 1185,0 | 2252,5 | 2267,5 | 1622,5  MHz

At some boards I can't see a LO signal in the range of 1GHz to 4GHz  ( LO output driver = always enabled ).

SPI signals: the SPI clock frequency is about 2MHz, delay from LE =low to first clock is arround 1.2 to 1.3 us.

LE idle = 'high' / clock idle = 'low'  / data: MSB first

OK - are there any changes by the used ADRF6602 chips?  Are there any helpful hints for me?

Best regards

BroadBand-01