Post Go back to editing

ADF4212L power up sequence through rate 2

My customers have problems with powering on the ADF4212L.
We found the following thread looking for an answer.

 

ADF4212L power up sequence through rate

https://ez.analog.com/thread/13793

 


The thread says "As a first-hand advice, i would like to ask you to clear all bits (programm to 0) in Register 0 (IF R counter latch) and write 0x2 to Register 2 (RF R counter latch) after the part is powered up, and only after that is done to write all you register with current settings. "
This was a wonderful answer for my customers.

So please allow me small questions.
Does the MPU require waiting time when executing the above command?

If necessary, how long is the time?

Best regards

Parents
  • Hello,

    The MPU should wait until the ADF4212L has powered up ...I.e  the supply voltages should be VDD1 = VDD2 = 2.7 V to 3.3 V; VP1, VP2 = VDD to 5.5 V;

     

    Once the supplies have settled, then you can write to the part to clear the registers as indicated in the previous thread.

     

    regards,

    Brigid.

     

Reply
  • Hello,

    The MPU should wait until the ADF4212L has powered up ...I.e  the supply voltages should be VDD1 = VDD2 = 2.7 V to 3.3 V; VP1, VP2 = VDD to 5.5 V;

     

    Once the supplies have settled, then you can write to the part to clear the registers as indicated in the previous thread.

     

    regards,

    Brigid.

     

Children
No Data