Hi all, Can i use ADL5513 with suppyling power to only one VPOS pin?
ADL5513
Recommended for New Designs
The ADL5513 is a demodulating logarithmic amplifier, capable of accurately converting an RF input signal to a corresponding decibel-scaled output. It employs...
Datasheet
ADL5513 on Analog.com
Hi all, Can i use ADL5513 with suppyling power to only one VPOS pin?
Each VPOS pin goes to a dedicated bond pad on the die. I do not know if they are electrically connected on the die. Even if they were connected, I would advise not to connect the ADL5513 in this manner as poor reliability could result. Please follow the connection recommendations in the PIN CONFIGUATION AND FUNCTION DESCRIPTION section of the datasheet.