LT5560 component :0.01MHz to 4GHz Low Power Active Mixer......

.Please tell me the impedance of LO input at 10MHz and also the value of the components(C3,C4,C5,L5) required for the  reactive matching at this frequency

LT5560-0.01MHzto4GHzLowPowerActiveMixer.pdf
Parents
  • Thanks for the information.

    For my application the signal output port(Pin 5&6) frequency range is from 1KHz to 20KHz, so according to Table7 & Figure 3 its working for 10MHz with L3=L4=0 i.e. no external component is required, only transformer is required for impedance matching.

    So, "will this configuration work for 1KHz-20KHz (much lower frequency) output"

    No information is available for such lower frequency IF output in the datasheet.

Reply
  • Thanks for the information.

    For my application the signal output port(Pin 5&6) frequency range is from 1KHz to 20KHz, so according to Table7 & Figure 3 its working for 10MHz with L3=L4=0 i.e. no external component is required, only transformer is required for impedance matching.

    So, "will this configuration work for 1KHz-20KHz (much lower frequency) output"

    No information is available for such lower frequency IF output in the datasheet.

Children
No Data