LT5560 component :0.01MHz to 4GHz Low Power Active Mixer......

.Please tell me the impedance of LO input at 10MHz and also the value of the components(C3,C4,C5,L5) required for the  reactive matching at this frequency

LT5560-0.01MHzto4GHzLowPowerActiveMixer.pdf
Parents
  • Typically, RF components are simulated using s-parameters and signal chain characteristics (gain, IP3, NF, etc.), not their time-domain characteristics.

    To do this, you would use an RF simulator such as ADS or QUCS for the s-parameters, and any number of programs to do a signal chain analysis. One that I like to use is AppCad.

Reply
  • Typically, RF components are simulated using s-parameters and signal chain characteristics (gain, IP3, NF, etc.), not their time-domain characteristics.

    To do this, you would use an RF simulator such as ADS or QUCS for the s-parameters, and any number of programs to do a signal chain analysis. One that I like to use is AppCad.

Children
No Data