Post Go back to editing

HMC557A as an Upconverter

Thread Summary

The user requested a spurious performance table for the HMC557A in an up conversion setup with LO at 4 GHz, IF input from 120 to 600 MHz, and RF output from 4.1 to 4.6 GHz. The provided reference table shows spur values for RFout at 5 GHz and IF input at 100 MHz, with IF input power at -10 dBm. The user is advised to verify specific frequency plans using an Evaluation Board.
AI Generated Content

Hello all,

In the HMC557A data sheets there is a spurious performance table for the standard down conversion case.

Can you please provide a similar table but for the up conversion case (i.e. input is the IF port, Output is the RF port).

Any up conversion table will help me but I am interested specifically in the following frequency ranges:

Lo: approx. 4 GHz.

IF input: 120 to 600 MHz

RF output: 4.1 - 4.6 GHz

Thank you for the prompt response

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.