Post Go back to editing

ADRF6720-27

I have a problem with the output power of ADRF6720-27, It's output power is about -16dbm while in datasheet said it is about 0dBm. i read and checked all registers and input power of baseband inputs and i think they are OK. Can anyone help me to improve the output power? Should i enable anything else?

Thanks.

ref input: 50MHz

PFD: 25 MHz

Output Freq: 2550MHz

BaseBand : 10MHz, 1 Vp-p

  • Sorry for missing this question for long time.

    If you still have an issue at the lower output power, can you capture baseband input signals(I+/I-/Q+/Q-) by oscilloscope? And if possible, can you also capture rf output spectrum?  If baseband inputs are 1Vp_p at 2.7 V biased and set the registers correctly(especially reg.0x30 = 0x0000), it should be around 2.9dBm.

    Thanks

    Tony

  • This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin