Post Go back to editing

HMC856 Eval board Interfacing

Thread Summary

The user is trying to interface the B0-B4 control ports of the HMC856 eval board to an LVTTL (1.8, 2.5, or 3.3V) control system. The final answer confirms that VT should be tied to GND. However, the eval board has 600 Ohm internal pull-ups connected to VT, and the VT-J8 pin is floating, which contradicts the user's initial assumption. The user seeks clarification on the correct configuration for B0-B4 with LVTTL signals.
AI Generated Content

I am reviewing the HMC856 eval board schematic on page 12 of the HMC856 data sheet.  I am trying to figure out how to interface the control (B0-B4) to LVTTL (1.8, 2.5 or 3.3V) control system.  Is it possible?