Hi, I have a HMC739LP4 evaluation board, which I want to use to setup a heterodyne phase locked loop. I wanted to know the fastest speed/frequency or response time, upto which I can tune the input voltage signal ? This is important for me, since I need to know if this VCO is suitable for my application. For e.g. Can I frequency modulate the (input voltage of the) VCO and achieve datasheet performance for a MHz range input voltage signals ? I have a tunable loop-filter that works upto 200 MHz. This information isn't present in the datasheet as far as I understand. Thanks...