Post Go back to editing

output pull-up inductor for 700MHz to 1.5GHz

Thread Summary

The user inquired about a suitable output pull-up inductor for the ADF4382 over the 700 MHz to 1.5 GHz frequency range. The final answer confirmed that the LQW15AN1N4C1ZD, with an impedance of about 6 ohms at 700 MHz and 13 ohms at 1.5 GHz, is still appropriate but may result in marginally lower output power. Larger-value inductors, around 30 nH, were suggested for maximizing output power, though no specific part numbers were recommended.
AI Generated Content
Category: Hardware
Product Number: ADF4382

Hi ADI

Please can you recommend an output pull-up inductor, as per your datasheet figure 66, for maximum output power for the ADF4382 for use over the frequency range 700MHz to 1500MHz?

Thanks

JP

Parents
  • Hi JP,

     

    You are correct that the impedance of the LQW15AN1N4C1ZD is about 6 ohms at 700 MHz and 13 ohms at 1500 MHZ. While the 1.4 nH inductor presents a lower impedance at your frequency range, the ADF4382 will still operate correctly posing only a marginally lower output power. 

     

    If maximizing output power in the 700 MHz to 1.5 GHz band is critical for your design, you could evaluate using a larger-value pull-up inductor, upwards of ~30 nH, however, I cannot recommend a specific alternative part number outside of what has been tested and validated by the product engineers. 


    Best,
    Hayden

Reply
  • Hi JP,

     

    You are correct that the impedance of the LQW15AN1N4C1ZD is about 6 ohms at 700 MHz and 13 ohms at 1500 MHZ. While the 1.4 nH inductor presents a lower impedance at your frequency range, the ADF4382 will still operate correctly posing only a marginally lower output power. 

     

    If maximizing output power in the 700 MHz to 1.5 GHz band is critical for your design, you could evaluate using a larger-value pull-up inductor, upwards of ~30 nH, however, I cannot recommend a specific alternative part number outside of what has been tested and validated by the product engineers. 


    Best,
    Hayden

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.