Hi ADI
Please can you recommend an output pull-up inductor, as per your datasheet figure 66, for maximum output power for the ADF4382 for use over the frequency range 700MHz to 1500MHz?
Thanks
JP
KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
ADF4382
Recommended for New Designs
The ADF4382 is a high performance, ultra-low jitter, fractional-N
phased-locked loop (PLL) with an integrated voltage controlled
oscillator (VCO) ideally...
Datasheet
ADF4382 on Analog.com
Hi ADI
Please can you recommend an output pull-up inductor, as per your datasheet figure 66, for maximum output power for the ADF4382 for use over the frequency range 700MHz to 1500MHz?
Thanks
JP
Hi JP,
I recommend that you use the LQW15AN1N4C1ZD from Murata Electronics as your output pull-up inductor to achieve maximum output power. This is the same pull-up inductor that we use on the EV-ADF4382SD1Z evaluation board.
Let me know if you have any other questions.
Regards,
Hayden
Hi Hayden
Thanks for replying. I'm not sure that the LQW15AN1N4C1ZD will be suitable for 700MHz since at these frequencies the impedance of the inductor is about 6 ohms according to the LQW15AN1N4C1Z# website. Can you confirm?
Thanks
JP
Hi JP,
You are correct that the impedance of the LQW15AN1N4C1ZD is about 6 ohms at 700 MHz and 13 ohms at 1500 MHZ. While the 1.4 nH inductor presents a lower impedance at your frequency range, the ADF4382 will still operate correctly posing only a marginally lower output power.
If maximizing output power in the 700 MHz to 1.5 GHz band is critical for your design, you could evaluate using a larger-value pull-up inductor, upwards of ~30 nH, however, I cannot recommend a specific alternative part number outside of what has been tested and validated by the product engineers.
Best,
Hayden