Post Go back to editing

1 GHz bandwidth in L-Band (1-2 GHz) and S-Band (2-4 GHz)

Category: Datasheet/Specs
Product Number: LTC5510

Hi, I am looking for a mixer that can up or downconvert a 1 GHz wide signal in the 250 MHz to 6 GHz frequency range. With a proper balun and/or other matching external to LTC5510, can this be achieved? I am guessing in most cases the balun selects the frequency range and that the mixer itself doesn't have any bandwidth limitation. Is that correct? If not, what kind of fractional bandwidth can this part achieve if external matching allows anything between 1 MHz to 6 GHz to pass through? Thanks.

  • Hello,

     

    Apologies for the delay in response, I am still in the process of creating a proper test configuration for this mixer. As I am attempting to apply a 1 GHz wide signal onto this component, I'm first trying to ensure that the instrumentation I have available in our lab can actually output that range withing the frequency spectrum of interest. One of our signal generators is limited in its top end frequency range at around 4 GHz, as well as in bandwidth, around 800 MHz, but I am very much still exploring options in order to hopefully build a more accurate source and test configuration for this mixer to obtain representative data.

     

    I'll be sure to update you if there are any developments along the way.

     

    Best regards,

  • Hi, you don't need a 1 GHz wide signal for this measurement. You can fix the LO frequency and sweep the input frequency over a 1 GHz bandwidth with a CW tone, stepping in 100MHz steps as shown in the Table below. The main parameters of interest are:

    1. Conversion gain vs input (or output) frequency.
    2. Spur table (at 1.5 GHz input and 3 GHz output frequency). High side LO frequency will be 4.5 GHz
    3. IN-OUT isolation
    4. LO-OUT leakage
    IF Freq - IN
    [MHz]
    LO Freq
    [MHz]
    RF Freq - OUT
    [MHz]
    RF Pwr
    [dBm]
    Conv Loss
    [dB]
    1000 4500 3500    
    1100 4500 3400    
    1200 4500 3300    
    1300 4500 3200    
    1400 4500 3100    
    1500 4500 3000    
    1600 4500 2900    
    1700 4500 2800    
    1800 4500 2700    
    1900 4500 2600    
    2000 4500 2500    

    Please let me know if you have any question. I think DC1983A is the most appropriate demo circuit for the above measurements. Please use a supply voltage of 5 V for this measurement.

    Thank you so much for your help.

    Best Regards,

    Noman

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.