i am facing an issue with determining the Lockin time of the ADF4372. Currently using the Eval Board, and the ACE software to input and change configuration of the device. I am also unable to change the Muxout mode from DLD and Data. Anytime i try to change the mode (for ex. High and Muxout or DLD and Muxout) and then click on Initialise/Write all registers, it reverts back to DLD and Data and i dont get any output. I am not facing any issues when i do the same with ADF4356 Eval Board.
And also when I input a different frequency and Initialise/Write all registers i get the image (attatched) as the output from the Muxout pin. I dont see why i keep getting the the two spikes instead of a proper square wave in ADF4356. Please help me out