Post Go back to editing

Questions Regarding ADAR3000 16-Beam/16-Element Scalable Architecture

Thread Summary

The user inquires about the ADAR3000/ADAR3001 multi-beam beamformer architecture, specifically how four ADAR3000 devices are combined to form a 16-beam/16-element phased array. The final answer indicates that a conceptual diagram or PCB layout will be provided to clarify the implementation. The user also asks if the four RF inputs of each ADAR3000 can operate at the same carrier frequency and if there is a reference design for one tile.
AI Generated Content
Category: Hardware
Product Number: ADAR3000

I am studying the ADAR3000/ADAR3001 multi-beam beamformer architecture described in the application note "Low SWaP Ka-Band Beamforming ICs for SATCOM Payloads" and would appreciate clarification regarding the scalable 16-beam/16-element implementation.

The application note states that four ADAR3000 beamformer ICs can be combined to realize a 16-beam/16-element phased array. I understand that each ADAR3000 accepts four RF beam inputs and produces four outputs corresponding to four antenna elements. However, I am uncertain about the physical RF implementation of one tile.

Specifically, I would appreciate clarification on the following points:

  1. For one 4-element tile, are the four outputs corresponding to the same antenna element from the four ADAR3000 devices physically combined using an external 4:1 Wilkinson combiner before feeding the PA and antenna element?
  2. If so, could you provide a conceptual diagram or PCB layout showing how one complete tile (4 ADAR3000 + 4 combiners + 4 antenna elements) is implemented?
  3. In the 16-beam example, do the four RF inputs of each ADAR3000 correspond to four independent frequency channels, or can they operate at the same RF carrier frequency? If they can share the same carrier, how are the beam signals kept independent after the external RF combiners?
  4. Is there any reference design, evaluation board layout, or additional application note that illustrates the complete RF routing for one tile?

I would like to understand the intended implementation of the ADAR3000 architecture before proceeding with my own design.

Thank you very much for your assistance.

Edit Notes

Paraphrased the last sentence.
[edited by: Sirous at 1:32 AM (GMT -4) on 3 Aug 2026]
Parents
  • There is more than one way to do this. The key point is that there must be a path for all 16 input beams to all 16 elements. In the first example below, all 16 beams route to the first blade (Blade 0). This means that Element 0, Element 1, Element 2 and Element 3 (antennae), all have a path back to the 16 beams. 

    You also have to route all 16 beams to Blade 1. This happens at the output of the first line of splitters. 

    Here is another approach. You could instead just route Beams 0, 1 2 and 3 to Blade 0 (Beams 4,5,6 and 7 go to Blade 1, etc). In this case the output wiring needs to be different so that all 16 beams have a path to each output beam. 

    I don't have a conceptual PCB layout or reference design for either of these approaches. 

    Regarding having channels at the same frequency, I'm less certain about that. I think that if you have two beams at the same frequency, the system can accommodate this if the two beams are pointed in different directions (say in a transmitter). If they are pointed in the same direction, I think that this will be problematic. 

Reply
  • There is more than one way to do this. The key point is that there must be a path for all 16 input beams to all 16 elements. In the first example below, all 16 beams route to the first blade (Blade 0). This means that Element 0, Element 1, Element 2 and Element 3 (antennae), all have a path back to the 16 beams. 

    You also have to route all 16 beams to Blade 1. This happens at the output of the first line of splitters. 

    Here is another approach. You could instead just route Beams 0, 1 2 and 3 to Blade 0 (Beams 4,5,6 and 7 go to Blade 1, etc). In this case the output wiring needs to be different so that all 16 beams have a path to each output beam. 

    I don't have a conceptual PCB layout or reference design for either of these approaches. 

    Regarding having channels at the same frequency, I'm less certain about that. I think that if you have two beams at the same frequency, the system can accommodate this if the two beams are pointed in different directions (say in a transmitter). If they are pointed in the same direction, I think that this will be problematic. 

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.