Post Go back to editing

ADF4382 Output Amplitude Register

Thread Summary

The user inquired about the mapping of RFOUTx_OPWR settings to output power in the ADF4382. The support engineer provided characterization data showing output power versus RFOUTx_OPWR code (0–15) at 15 GHz, noting that power settings above 11 do not yield higher output power and can be unstable. The data includes a plot of output power vs frequency for power setting 11.

View FAQ
AI Generated Content
Category: Hardware
Product Number: ADF4382

I'm using the ADF4382 and have a question about register 0x29 (RFOUTx_OPWR). The datasheet shows output power measurements for specific RFOUTx_OPWR settings, but I couldn't find any information describing how the RFOUTx_OPWR setting maps to output power. Could you provide characterization data showing differential output power versus RFOUTx_OPWR code (0–15) or approximately how much output power changes per code step?

  • I'm attaching some data taken with the ADF438A evaluation board. Note that the measurement was not de-embedded. So the power reference plane is the SMA connector on the board. The file includes a plot of output power vs frequency for power setting 11 along with a sweep of output power vs power setting at 15 GHz. It's not explicitly stated in the datasheet but our recommendation is not to use power settings above 11. You can see in the power sweep that the output power at setting 12 drops relative to setting 11. It comes back up at settings 13, 14 and 15.  But you do not get higher power than setting 11. So the simplest thing to do is stop at 11. 

      

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.