Hi everyone,
Recently I have been trying to work with ADF4382A an its evaluation board (EVAL-ADF4382A, REV D) both with ACE software and my own C functions and I am having some problems.
At first I was only trying to write and read through the SPI with my own custom C functions and while the writing operations seemed to work pretty well, the reading ones failed as the values read didn't match with the expected ones. I am sure that the registers were written ok because with an oscilloscope I could see the SDIO line change its voltage depending on the configuration of the 0x3D register. I could even achieve the PLL lock at some frequency of my interest. But, unfortunately, when I tried to make a silly read operation following the datasheet instructions, I encountered that the values returned were wrong. I tried to read different registers like 0x0C or 0x0D but instead of returning the POR values they returned 0x01 and 0x00.
I assumed that my code had some mistake coming from a missunderstanding so I decided to use ACE to make some reads and compare the oscilloscope readings with the previous ones. To my surprise, the readings returned the same (e.g. 0x01 from the 0x0C register). This happens in spite of the SPIO line configuration, whether I use 3 or 4 wires, 1.8 or 3.3 V. In the screenshot of the oscilloscope trace that is attached I was working with 4 wires and 1.8V using ACE software. (BLUE = CSB, RED = SCLK, GREEN = SDO, YELLOW = SDIO)

I have not much knowledge, but I can see some things that for me seem off:
1- If the PLL is working in 1.8V, why does the logich high of the SDIO line reach 2.65V?
2- Is it normal that the SDO line is stuck at 2.36V when writing the address? Because when performing the reading at logic high it only reaches 1.8V
I have read across EF that there used to be a problem with a SDO resistor with some revisions of the evaluation board, but the bad readings for me also happen in the 3 wire configuration, so it may not be just a SDO problem, right? (see 2nd screenshot, 3wire 3.3V)

For me this seems like some kind of electrical problem, but I don't know how could this be when I am working with the EVAL board and the SDP-S controller board. Does anyone have some ideas?
Thank you very much in advance,
Andres