I'm trying to enable the Q channel in a MAX2769B. Using either device state 2 or device state 6 as a baseline, the configuration messages provided in the data sheet do not appear to be correct. What set of configuration messages should I use to enable the Q channel from a baseline device state of 2 or 6 in a MAX2769B?
Edit Notes
Wanted to clarify that I know device state 2 and 6 are I only. I want to clarify that I'm using those device states as reference for the desired output which is based on what device state 2 and 6 are, but with Q channel enabled.[edited by: KyleG at 10:49 PM (GMT -4) on 28 Jun 2026]