Hi all. I have used this switch before. In my latest design it shows nearly the same 30dB loss (S21) in both RF1 to RFC and all ports terminated. I'm using RF1 and RF2 as inputs and RFC as an output. The switch selects between two paths and outputs the desired one to RFC, a coupling cap and then an output SMA connector. My S11 and S22 also look lousy on my network analyzer. I'm testing from 1MHz to 4GHz. I'm using 3.3V Power supply. I have C L C filters on the CTRL and EN lines. I don't suspect this is a problem. I have probed voltages on IC side of filters and levels look correct enough to trigger desired switch state.
The bold line is in RF1-to-RFC mode. The lighter line is in all-ports-terminated or off mode. The X-axis marks are cutoff but it's a linear scale 1MHz to 4GHz.
S21:

S22:

S11:

Time Domain makes it look OK until it gets to this switch. This plot shows it with the switch completely removed from the board vs installed and in RF1-to-RFC mode AND in all-ports-terminated mode.

Here's the schematic of the area. Powered down, on switch side of coupling caps I get 70-80 ohms DCR to ground with fluke DMM. I've tried pulling the ESD diodes -- it doesn't change anything.

Thoughts? My previous design used 5V psu and no filtering on the control lines. I really don't see how this could make a difference. Hoping someone has experience with this failure mode and can comment. Thanks for your help!