Post Go back to editing

3.3V power supplies

Thread Summary

The user inquired about using a single LDO to power both 3.3 V supply groups of the ADF4382 PLL. The final answer indicates it is possible but may degrade phase noise due to noise coupling. Recommendations include using separate filtering or ferrite beads to isolate the sensitive (VCO, OUTDIV, RFOUTx) and digital/PFD groups, with a maximum 0.3 V drop. The accompanying answer suggests using a dual-output LDO like the LT3029 or MAX25307, or a small single LDO like the MAX38902 to address space constraints.
AI Generated Content
Category: Hardware
Product Number: ADF4382

Hi team,

i'm using the PLL ADF4382 for a new project.

I read in the datasheet and the user guide that the +3.3 V power supplies are divided into two separate groups, each powered by its own dedicated LDO.

Would it be possible to use a single LDO to supply both groups? 

Would any phase noise degradation be expected if a single LDO were used to supply both groups?

Thank you in advance.

Best Regard,

Matteo Ricci

Parents
  • Hi,

    thank you for the answer.

    To keep the two voltage groups separated, would it be possible to use a dual-output LDO while keeping good phase noise performance? If so, could you suggest a possible part number?

    We have space constraints, so it would be important to avoid using two separate LDOs.

    Thank you,

    Matteo

Reply
  • Hi,

    thank you for the answer.

    To keep the two voltage groups separated, would it be possible to use a dual-output LDO while keeping good phase noise performance? If so, could you suggest a possible part number?

    We have space constraints, so it would be important to avoid using two separate LDOs.

    Thank you,

    Matteo

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.