Post Go back to editing

2.4GHz input frequency

Thread Summary

The user inquired about using the LTC5576 RF mixer at 2.4 GHz, despite its specified range of 3 GHz to 8 GHz. The support engineer advised that conversion gain and OIP3 would be poor at 2.4 GHz and suggested considering the LTC5562, which covers ISM applications up to 7 GHz. The user provided the location as Livermore, CA, for potential field support.
AI Generated Content
Category: Datasheet/Specs
Product Number: LTC5576

I am looking for RF mixer that will operate at 2.4GHz and 5.6GHz. LTC5576 specifies 3GHz - 8GHz frequency range for RF input signal.

Will it operate at 2.4 GHz with reduces performance and which parameters will be compromised?