Post Go back to editing

Fast cal setup

Thread Summary

The user asks if R=3 is required to achieve an integer value for 10GHz calibration with a 120MHz reference frequency. The final answer confirms that dividing the phase detector frequency to 40MHz is necessary for fast calibration at 10GHz. An alternative is to use Nmin=84 for a minimum frequency of 10.08GHz if 10GHz is not strictly required.

View FAQ
AI Generated Content
Category: Hardware
Product Number: ADF4383

In AN-2623, steps 5 and 6 describe calculating an integer N to calibrate for 10GHz, the lowest calibration frequency. No fractional word should be entered: 

In the case of 120MHz reference, will we have to set R=3 so that 40MHz will yield an integer value?

Parents Reply Children
No Data