Post Go back to editing

ADRF5162 low frequency range

Thread Summary

The user inquires about the ADRF5162's derating at low frequencies (400 MHz) for an application requiring a 0.4-3 GHz antenna switch with 44 dBm pulsed RF power. The final answer explains that the derating is due to voltage and current stress limits on the FETs, not lower power compression, and that P1dB decreases at lower frequencies but the max input power limitation drops faster. Good thermal management may help, but the max input power spec remains a critical constraint.

View FAQ
AI Generated Content
Category: Hardware
Product Number: ADRF5162

Hi,

We are considering ADRF5162 for an application requiring an antenna switch in 0.4-3GHz range and 44dBm power. The RF power is pulsed with maximum on duration of 500us and repetition rare of 1KHz.  Going through data sheet, fig.9-12 show excellent performance all the way down to very low frequencies. But fig. 2 tells another story. I understand perfectly well the need to derate at high frequencies as the loss increases but what’s the reason for derating at low frequencies, at 400MHz (which is advertised as working frequency) the derating is almost -7dB!  Is the need to derate related lower power compression?  Do you have any number on P1dB at low frequencies? If we can accept higher harmonics can the device be used with good thermal management?

Regard/ Ramin

  • The derating spec on RF input power that kicks in at 1 GHz is driven by voltage and current stress limits on the FETs in the device. The limit is not put in there because the input compression point is degrading at lower frequency. However from looking at datasheet plots of other devices that have a derated max input power spec at lower frequencies, I see that some of this include plots of P1dB and IP3 which show it decreasing. So while your input power is bound for safety reasons, you can also expect the P1dB to decrease. However, I think that the max input power limitation will drop faster than the input compression. So in a sense, it doesn't really matter what the P1dB spec is below 1 GHz. 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.