Post Go back to editing

500 MHz bandwidth application

Thread Summary

The user asked if the ADRF6821's 500 MHz bandwidth is single-side or double-side. The final answer clarifies that the 500 MHz is the complex baseband (I/Q) bandwidth at the demodulator output, allowing for an RF signal of up to 1 GHz (±500 MHz) around the LO to be translated to baseband.
AI Generated Content
Category: Datasheet/Specs
Product Number: ADRF6821

ADRF6821 documentation specify its bandwidth value as 500 MHz. Is this the "single-side bandwidth" or "double-side bandwidth"?

  • The ADRF6821’s specified 500 MHz “demodulation/baseband bandwidth” is the complex baseband bandwidth after downconversion, i.e., the bandwidth of the I/Q (baseband) outputs around DC. At RF, the corresponding instantaneous RF bandwidth can be up to approximately double this value, because a real RF signal centered at the LO maps its positive and negative frequency sidebands into the complex baseband.

    In practical terms, this means:

    • The 500 MHz figure is the usable complex baseband (I/Q) bandwidth at the demodulator output.

    • An RF signal occupying about 1 GHz of real passband around the LO (±500 MHz) can in principle be translated to baseband, appearing as a 500 MHz complex baseband signal at I/Q. This aligns with internal support guidance that “500 MHz is the bandwidth when the signal is down-converted to baseband. At the RF input the instantaneous bandwidth could be double.” 

    .

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.