Hello all,
We currently use the ADF4371 on a design where a microcontroller on another board communicates with it via SPI.
We are struggling to get it to work.
We can drive the ADF4371 evaluation board with our control board but ONLY if we use the 1.5k resistors on the clock or data lines.
Our clock speed is about 1 MHz.
Are these resistors necessary and wouldn't this limit higher clock rates.
The datasheet does not mention using them but we literally cannot get the eval board to work if we drive the SPI directly from the microncontroller.
We have also historically had assembly issues with these ICs. We have used the same footprint as on the eval board but the assembly houses are struggling to get them down correctly which adds another variable to the fault finding process.
Any footprint/ assembly suggestions?
kind regards
Steve