Post Go back to editing

ADF4382A RF output power in divide-by-2 and divide-by-4 modes

Thread Summary

The user inquired about RF output power data for the ADF4382A in the divide-by-2 (5.75GHz-10.5GHz) and divide-by-4 (2.875GHz-5.25GHz) ranges, and process variation (min/max power). The final answer provided a plot showing RF output power from 5 to 21 GHz, noting that operation is not guaranteed below 2.875 GHz, between 5.25-5.75 GHz, 10.5-11.5 GHz, and above 21 GHz. The plot aligns with the datasheet's typical output power data and includes performance over temperature.

View FAQ
AI Generated Content
Category: Hardware
Product Number: ADF4382A

Hello,

The ADF4382A datasheet only specifies RF output power in the fundamental output frequency range of 11.5GHz to 21GHz (figure 24). Do you have any data on the RF output power between 5.75GHz-10.5GHz (divide-by-2 range) and 2.875GHz-5.25GHz (divide-by-4 range)?

The datasheet also only specifies typical output power. Do you have any data on likely process variation (i.e. minimum and maximum power)?

Thank you.