Post Go back to editing

HMC305s insertion loss

Category: Hardware
Product Number: HMC305S

Hello,

I am currently evaluating the HMC305S digital attenuator and I am observing unexpected insertion loss behavior.

Test setup:
- Standalone HMC305S measured with a VNA
- No control interface activity during the initial measurement

Observed behavior:
- Device unpowered (VCC = 0 V): insertion loss ≈ 15.5 dB (signal passes through the device)
- Device powered (VCC applied, no control activity): insertion loss ≈ 21.5 dB
- Device powered with SPI control: attenuation range ≈ 6–21.5 dB

It appears that the entire attenuation range is shifted by approximately +6 dB compared to the expected 0–15.5 dB range specified in the datasheet.

My questions:

1. What is the expected default attenuation state at power-up if the control pins are left floating?
2. Do the control inputs have internal pull-up or pull-down resistors that could result in a non-zero default attenuation state?
3. Are there specific pin biasing or power-up sequencing requirements needed to achieve the datasheet-specified minimum insertion loss?
4. Is a +6 dB offset consistent with normal device operation?

I can provide additional details (frequency, supply measurements, PCB layout, etc.) if needed.

Thank you in advance for your support.

Parents
  • Hello Arthur,

    I can help you with your query. You need at least a function generator to drive the serial data into the device.

    1- Device sets itself to maximum attenuation when pins are left floating, 15.5dB, plus the reference Insertion loss, about 17dB.

    2- As answered above, device sets itself to maximum attenuation to avoid certain scenarios.

    3- You need to drive 2 square waves for i) Clock ii)Latch Enable, as the data is written into the IC at the rising edge of LE. For 5V supply, 5V control signals, while noticing that control pins have high-Z, so your function generator should mimic that to avoid voltage doubling. You can just connect 5V or 0V at Serial Input, 0V for max attenuation(default), 5V for Insertion Loss(minimum state), at the rising edge of each Latch Enable, your Serial Input is then written into registers. 100Hz LE square signal with 1khz clock square signal was enough for me on test bench.

    4- Device has about 1.5-1.7dB insertion loss, 6dB is not reasonable.

    Kind Regards,

    Turgut Ersöz

    ADEF-Comms Applications Team

Reply
  • Hello Arthur,

    I can help you with your query. You need at least a function generator to drive the serial data into the device.

    1- Device sets itself to maximum attenuation when pins are left floating, 15.5dB, plus the reference Insertion loss, about 17dB.

    2- As answered above, device sets itself to maximum attenuation to avoid certain scenarios.

    3- You need to drive 2 square waves for i) Clock ii)Latch Enable, as the data is written into the IC at the rising edge of LE. For 5V supply, 5V control signals, while noticing that control pins have high-Z, so your function generator should mimic that to avoid voltage doubling. You can just connect 5V or 0V at Serial Input, 0V for max attenuation(default), 5V for Insertion Loss(minimum state), at the rising edge of each Latch Enable, your Serial Input is then written into registers. 100Hz LE square signal with 1khz clock square signal was enough for me on test bench.

    4- Device has about 1.5-1.7dB insertion loss, 6dB is not reasonable.

    Kind Regards,

    Turgut Ersöz

    ADEF-Comms Applications Team

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.