Hi,
Can you please provide the IP2 for SP4T switch ADRF5050 from 30 to 6000MHz frequency range.
ADRF5050
Recommended for New Designs
The ADRF5050 is a nonreflective SP4T switch manufactured in a silicon on insulator (SOI) process.
The ADRF5050 operates from 100 MHz to 20 GHz with insertion...
Datasheet
ADRF5050 on Analog.com
Hi,
Can you please provide the IP2 for SP4T switch ADRF5050 from 30 to 6000MHz frequency range.
I don't have a dataset to provide buy my colleagues back at the factory tell me that the 110 dBm number for IP2 holds up down to 100 MHz. Below 100 MHz, which is outside of the specified operating frequency range of the device, we would expect some roll-off in IP2 similar to what you see in Figure 25 in the datasheet.