Hello support team,
I am planning to use ADL5801 mixer (same circuit) for below combinations.
1. RF input : 30-88 MHz , LO : 140.7 to 198.7 MHz, IF : Fixed 110.7 MHz
2. RF input : 225-520 MHz, LO: 114.3 to 409.3 MHz , IF : Fixed 110.7 MHz
3. RF input : 30-88 MHz , LO : 793.5 to 851.5 MHz, IF : Fixed 881.5 MHz
4. RF input : 225-520 MHz, LO: 369.5 to 656.5 MHz , IF : Fixed 881.5 MHz
There will be one SPDT switch at the IF port , which will further route wither 110.7 MHz or 881.5 MHz.
Now, out of these 4 combinations, 3 combinations have IF > RF (1, 3, 4), but one combination has IF< RF(2), so for RF and LO port, I am selecting a wideband balun 10-6000 MHz, but for IF port, none of the suggested balun suffice these combinations. so can you suggest a suitable IF balun for the same. also, kindly review above combinations and share feedback