When adjusting Vneg and Vgate_threshold on the HMC981LP3E, are resistors always required in both feedback paths, or can Vgate_threshold be adjusted while Vneg remains at its default value of -2.5V?
I want to use the HMC981LP3E to bias a Mini-Circuits AVA-183MP+. The bias requirements in its datasheet say it needs -2V Vgs to pinch off the channel, so I want Vgate_threshold set to -2V. The note in the spreadsheet calculator says I need a threshold at least 300 mV more positive than Vneg, so I thought no adjustment would be necessary for Vneg. I added a 1.5 Meg resistor to the R6 position on the HMC981LP3E eval board, but on startup the value of Vgate is pulled all the way down to Vneg(-2.5V). The examples I have seen for configuring this part tend to adjust Vneg and Vgate_threshold in tandem, but AN-1363 doesn't specify that this is required. Is my problem just that I didn't choose do adjust Vneg up by 100 mV along with Vgate_threshold?
To be clear, I don't have the amplifier connected because I don't want the excessive negative voltage to damage the gate, so I've considered that the missing headroom between Vgate_threshold and Vneg could just be the expected behavior under a no load condition. If that's the case, is there a recommended way simulate an amplifier under control and verify the HMC981LP3E is properly configured without connecting it to an expensive amplifier?