Post Go back to editing

Required configuration resistors for HMC981LP3E

Thread Summary

The user asked if resistors are required in both feedback paths when adjusting Vneg and Vgate_threshold on the HMC981LP3E. The support engineer confirmed that resistors are not always required in both paths, and the behavior observed (Vgate being pulled to Vneg) is expected under no-load conditions. The user verified the configuration by connecting the target amplifier (Mini-Circuits AVA-183MP+), and the issue resolved. The Vgate_threshold was slightly off, but the overall setup worked as intended.
AI Generated Content
Category: Hardware
Product Number: HMC981LP3E

When adjusting Vneg and Vgate_threshold on the HMC981LP3E, are resistors always required in both feedback paths, or can Vgate_threshold be adjusted while Vneg remains at its default value of -2.5V?

I want to use the HMC981LP3E to bias a Mini-Circuits AVA-183MP+. The bias requirements in its datasheet say it needs -2V Vgs to pinch off the channel, so I want Vgate_threshold set to -2V. The note in the spreadsheet calculator says I need a threshold at least 300 mV more positive than Vneg, so I thought no adjustment would be necessary for Vneg. I added a 1.5 Meg resistor to the R6 position on the HMC981LP3E eval board, but on startup the value of Vgate is pulled all the way down to Vneg(-2.5V). The examples I have seen for configuring this part tend to adjust Vneg and Vgate_threshold in tandem, but AN-1363 doesn't specify that this is required. Is my problem just that I didn't choose do adjust Vneg up by 100 mV along with Vgate_threshold?

To be clear, I don't have the amplifier connected because I don't want the excessive negative voltage to damage the gate, so I've considered that the missing headroom between Vgate_threshold and Vneg could just be the expected behavior under a no load condition. If that's the case, is there a recommended way simulate an amplifier under control and verify the HMC981LP3E is properly configured without connecting it to an expensive amplifier?

Parents
  • Hi Kyle, 

     

    The resistors are not required in both feedback paths, as long as the VGATE threshold is 300 mV more positive than VNEG. You should be fine with just placing 1.5 Mohms between VGATE and VGATEFB.

     

    Are you applying an enable signal to the HMC981? In the HMC980 datasheet, whose function is very similar to the HMC981, there is mention that “when EN is pulled down to ground, the HMC980LP4E discharges VDRAIN and VG2 down to ground and pulls the VGATE pin to VNEG. VGATE goes down to VNEG regardless of the threshold level setting of VGATEFB”. 

     

    The lack of amplifier on the output could also be causing this. Let me investigate this on my end and get back to you.

     

    Thanks,

    Joe

Reply
  • Hi Kyle, 

     

    The resistors are not required in both feedback paths, as long as the VGATE threshold is 300 mV more positive than VNEG. You should be fine with just placing 1.5 Mohms between VGATE and VGATEFB.

     

    Are you applying an enable signal to the HMC981? In the HMC980 datasheet, whose function is very similar to the HMC981, there is mention that “when EN is pulled down to ground, the HMC980LP4E discharges VDRAIN and VG2 down to ground and pulls the VGATE pin to VNEG. VGATE goes down to VNEG regardless of the threshold level setting of VGATEFB”. 

     

    The lack of amplifier on the output could also be causing this. Let me investigate this on my end and get back to you.

     

    Thanks,

    Joe

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.