Post Go back to editing

Configuration of TX Inputs for MAX2830

Thread Summary

The user inquires about using the MAX2830 for wireless audio applications, specifically if it can handle 0-20kHz analog signals. The final answer confirms the TX path can handle audio frequencies, but the RX path's HPF with a 100 Hz corner frequency will attenuate low-frequency signals. The support engineer advises against using the MAX2830 for this application due to potential distortion, as it is optimized for 802.11 standards.
AI Generated Content
Category: Datasheet/Specs
Product Number: MAX2830

Hello,

I plan on using the MAX2830 for a custom TX/RX pair for wireless audio applications, but im concerned if the chip can accept 0-20kHz on its TX pins. Does anyone with experience  using this chip know if I can feed low frequency analog into it?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.